Based on your location, we think there is a website better suited to you.

Tate Global AMER
Case Studies

YY London full structural refurbishment of original Canary Wharf office

Sector:
Commercial Office
Location:
Canary Wharf, London
Completion date:
September 2023
Architect:
Buckley Gray Yeoman

Canary Wharf’s 30 South Colonnade, now known as YY London demonstrates its sustainability efforts through its building design and function. Everyone involved had the responsibility of making sure this development became a new landmark of London.

Demonstrating sustainability through design

Working with main contractor, Skanska, the Tate team helped find a raised access flooring solution for the challenges they faced, resulting in the customer’s bespoke requirements being met.

A primary feature of this development is the giant floor-to-ceiling windows with a Y-shaped curved façade. This guaranteed that the 37,000 sq m of PSA:2021 medium grade RMG600 access flooring by Tate was a dynamic feature in its own right and complemented the professional office surroundings whilst remaining functional and adaptable. Tate raised access floor systems can be raised one panel at a time for precision and functionality when making required alterations in the underfloor void.

Supreme redesign, sustainably built for wellbeing

Like other projects in this area, harnessing innovation and being at the forefront of sustainability was important. Their sustainability objectives can be seen through many aspects of the development beginning at the design to the physical functionality and usage.

Installing our raised access floor systems in this development helped enable the office refurbishment to achieve a BREEAM Outstanding sustainable building certification. Two different systems were used for this project and both are supported by Environmental Product Declarations (EPD) that showcase these systems. The latest version of RMG600 (2023) has just 1.67 kg of CO2e per panel in modules A1 – A3 (product stage) of the product life cycle impact assessment (EN15804:2012 + A2:2019 update). The fusion of first-class design features with the retention of the existing structure, together with the sustainability efforts of this project have ensured that the development has achieved an overall saving of 10,260 tonnes of CO2.

The access floor systems that were used in this project were RMG600 and FDEB_H. RMG600 is a PSA:2021 Standard medium-grade system used in offices and FDEB_H is a PSA:2021 Standard heavy grade access floor used in data, IT, and plant rooms within the building.

The FDEB system is finished with a resilient surface covering that includes a High Pressure Laminate (HPL) architectural finish to control static. For this project, HPL was chosen because of its suitability within server rooms with a high volume of electrical equipment. Its intrinsic properties that dissipate static electricity make it extremely safe for these environments. It is also highly durable and resilient whilst still providing an attractive finish.

Gathering Inspiration from Location

It was a fantastic opportunity to be involved in a prestigious development in the heart of London’s Canary Wharf. The sustainability credentials of the building align with our own long-term Planet Passionate sustainability initiatives.

This development offers a cost-effective Environmental, Social and Governance (ESG) alternative to constructing new commercial buildings.

Frequently Asked Questions

YY London (formerly 30 South Colonnade) sits at the centre of Canary Wharf’s regeneration efforts.  The building has been transformed into a high-performance, wellbeing-focused workplace.

The redevelopment team, led by Skanska, ensured every aspect supported the project’s stringent ESG objectives.   It was awarded a BREEAM Outstanding rating and delivered more than 10,000 tonnes of CO₂ savings by retaining the existing structure, upgrading performance elements, and specifying low-impact materials.

Designed as a new architectural landmark, the building also incorporates extensive glazing to optimise natural light and elevate the user experience.

Two Tate flooring systems were installed, to meet differing performance requirements across the working areas, and offer reduced embodied carbon and circularity potential.

Tate’s market-leading RMG600 floor panel contains only 1.67 kg CO₂e per unit (A1–A3), contributing to the project’s low-carbon profile.  Furthermore, the system was able to adapt to the building’s dynamic, curved perimeter while also providing maintenance teams with easy access to underfloor building services.

For the building’s data and plant rooms, Tate’s Heavy Grade FDEB_H system with HPL finish provided both high load capacity and static control to protect sensitive equipment.

Both flooring systems have independently verified Environmental Product Declarations (EPDs).