Based on your location, we think there is a website better suited to you.

Tate Global AMER
Knowledge Articles

The future of office design: Flexibility, sustainability & employee well-being

New work practices and the rapid advancement of digitalisation across many business operations have fundamentally reshaped the employee experience and led to a re-evaluation of traditional office layouts. The design of office work environments is at the centre of a critical discussion about how companies should adapt to a rapidly evolving workplace.

Technology advancements are allowing companies to become more flexible, agile and support cross-team collaboration – the latter being particularly important for those adopting the hybrid working model (where employees spend at least 2-3 days/week in the office) where physical daily contact may be more limited. Rather than this reducing productivity, we’re seeing how investment in IT can support employees wherever they are based and enable seamless co-working.

Offices are being reconfigured to promote and support the new ways of working. Demand is rising for offices that are smaller, to accommodate a lower headcount at any one time, and more flexible, and companies are prioritising more face-to-face contact through initiatives such as creating more communal spaces in office buildings.

But that’s not the only trend. Recognising that offices are inevitably being compared to ‘home comforts’ for those used to working in their home office, many companies are improving on-site leisure, health, and well-being facilities, as well as investing in smarter decor.

Tate Future Office Design Knowledge Article Full Width Image Desktop En Uk

The rise of the luxurious offices

In major financial centres, such as London, this is being taken a step further. Smaller offices mean there has been more money to spend on luxury office accommodation - or, as The Economist reports, we’re seeing the rise of the uber-luxurious office.

Is this a long-term trend? It may be one that is at the mercy of macroeconomic trends - recessions and downturns have a habit of reining in any spending deemed to be non-critical. But there is little doubt that younger generations are more attracted to companies that focus on employee well-being.

Sustainability as a key priority

For many businesses, sustainability is as important as an improved employee experience, with great emphasis placed on minimising environmental impact, waste reduction, and the use of lower carbon materials in construction.

However, while new build standards are mandated, most offices are housed in ageing buildings which were built at a time when energy efficiency standards were considerably below where they are now.

According to a report published in April 2023 by Carter Jonas: 'Offices: Past, Present, Future', around a fifth of the UK office space fails to achieve current energy efficiency ratings that allows them to be let – that’s an Energy Performance Certification of at least E – although the report indicates that this figure may need to be treated with caution because some buildings will be exempt, and others may be being modified. Oxford, Cardiff and Edinburgh were reported as having the largest percentage of low rating offices, while only 28% of the country’s office stock was rated high quality, which is, as we’ve discussed, where the demand is currently highest.

Tate Future Office Design Citi Bank Knowledge Article Full Width Image Mobile En Uk

Citi Bank: A model for net-zero office refurbishment

Office refurbishment projects are, not surprisingly, extremely popular at the moment. Transforming existing office spaces into new workplaces, focused on improved user experience, and with low embodied carbon, are features of many of our most recent projects.

At Citi Bank’s Canary Wharf offices, we were contracted to support a project to reinvigorate the company’s 20-year-old office building as part of a full interior renovation.

The project delivered an agile, inspiring space that supports modern, hybrid, working practices and delivers against Citi Bank’s net-zero commitment.

It was conceived as a highly flexible space which could be quickly reconfigured to meet the needs of employees when they are in the office. As well as smart design, the renovations make innovative use of technology to drive cross-team creativity and collaboration.

Tate’s contribution: High-performance, sustainable raised flooring

It features Tate Hollow Floor, a system which is ideally suited to high-traffic areas. This tough, impact-resistant flooring can be used as a complementary system alongside floors which use steel-encapsulated panels - such as Tate RMG600+, our lowest ever embodied carbon raised access floor.

Both systems can be partnered with virtually any floor finish, including carpet, laminate, timbers, or vinyl, to create beautiful, inspiring designs.

Typically, Tate’s floor panels contain up to 75% recycled content without any compromise on their strength, integrity, or aesthetic quality. Plus, they are covered by our 25-year manufacturer’s warranty and fully tested to PSA: 2021 standards. We have a popular Take Back Scheme for any offcuts or waste material from our product, which we then recycle, ensuring they don’t end up in landfill.

We provide certified performance data, and verified environmental credentials and production claims, which are fully backed by independent evaluations and industry standards.

The project is due to be completed in 2025.

All Havas (HKX) images - David Churchill