Based on your location, we think there is a website better suited to you.

Tate Global AMER
Knowledge Articles

Third-party tested: New Tate Grid+ LEC

Tate Grid+ LEC is the next-generation lower embodied carbon ceiling solution from Tate.

With increased strength and load capacity, and a reduced carbon footprint through the use of lower embodied carbon aluminium, the new Tate Grid+ LEC offers an innovative solution that delivers significant advantages to data centre developers, architects, and installers. At the core of the product is an uncompromising focus on quality. Tate’s rigorous testing processes set the bar in testing standards, ensuring the reliability of the new optimised Tate Grid+ LEC.

Raising the bar in terms of testing, Tate Grid+ LEC has undergone the same precise testing as all of Tate’s product range, which includes:

Real-World Conditions: Tate conducts real-world tests by replicating a data centre ceiling environment at its Global Engineering Hubs. Full-scale tests are carried out on a specialised rig designed to simulate actual conditions, providing primary test evidence.

Independent Verification: Load assessment tests, fire rating tests, and pressure tests for air leakage are independently verified by third-party certified engineering consultants.

Vertical Tension Loads: The system undergoes rigorous vertical tension load testing, particularly focusing on its weakest point—the midspan of the unsupported structural tee. This testing helps determine the maximum working load capacity of the system.

Structural Integrity: A safety factor of 2 is applied, ensuring enhanced confidence in the system's performance.

Tate ensures a seamless customer journey with its Project Support, offering comprehensive assistance from the initial design and specifications stage to on-site visits from the project management team, who provide safety advice and guidance on installation, and offer both on-site and online training to support precise installation. This end-to-end approach delivers comprehensive support at every stage, with a committed focus on safety and performance.

Tate is committed to upholding the principles of ISO 9001, the internationally recognised standard for quality management systems. By fostering a culture of continuous improvement, Tate ensures that its products and services consistently meet customer and global regulatory requirements. This structured approach emphasises efficient processes, rigorous quality controls, and proactive risk management to enhance customer satisfaction and operational excellence. Tate prioritises stakeholder collaboration, regularly reviews performance, and integrates innovative solutions to maintain the highest standards of quality.

Designed with a higher grade of aluminium for added strength and engineered using LEC materials, Tate Grid+ LEC offers enhanced performance with a significantly increased maximum working load of 2.2kN.