As data-centre infrastructure becomes more complex, deployment approaches are evolving.
As data-centre requirements become more demanding, traditional infrastructure approaches can make design, coordination, procurement and installation increasingly challenging, while limiting flexibility for future expansion.
Konnect by Tate flips the traditional infrastructure model, shifting integration away from the project site and into a pre-integrated modular system. By bringing power, cooling, connectivity and supporting infrastructure together upstream, tangible benefits can be seen across five critical areas: time to market, complexity, cost efficiency, safety and scalability.
Time to Market
Traditional deployment can involve fragmented design, procurement and installation, considerably extending lead times. Our pre-integration of multiple elements – electrical busbars and tap-off boxes, RPPs and whips, liquid-cooling manifolds, CDU supply-and-return piping, fibre runners and cable-management infrastructure – results in a fundamentally different deployment model that dramatically reduces time to market.
Complexity
Bringing together products from multiple vendors can make traditional deployment more complicated, particularly where compatibility and coordination between systems are concerned. Konnect's single-source accountability combines traditionally separate mechanical and electrical infrastructure within a coordinated system, reducing the number of interfaces that project teams need to manage. Its design includes coordinated mechanical and electrical service alignment and an integrated cooling system combining manifolds and AHUs. This puts integration at the heart of the infrastructure design rather than leaving individual systems to be coordinated separately during deployment.
Cost Efficiency
Traditional installation processes can contribute to increased labour and material costs. Konnect is designed to reduce installation costs by moving more integration and coordination upstream. Features including roller arms, telescopic framing and adjustable mounts help optimise transportation, installation and site fit. Together, they demonstrate how transportation and installation have been considered as part of the infrastructure design itself.
Safety
Traditional deployment can require extensive on-site work, including activity at height. Konnect is designed to reduce on-site labour and the associated safety hazards through greater pre-integration. The physical design reinforces this approach. Telescopic legs use a ratchet-pin design for safe on-site lifting, while lift-ready columns are prepared for future hydraulic lift integration. How infrastructure is transported, lifted, positioned and connected forms part of the overall system rather than being treated solely as an on-site consideration.
Scalability
The final challenge is ensuring infrastructure can adapt as data-centre requirements change. While traditional designs can struggle to keep pace with AI-driven power and thermal demands, Konnect is designed to support the higher power densities and cooling requirements associated with AI and high-performance computing, while providing the modular flexibility to adapt as requirements evolve.
Contact us to learn more about how Konnect brings together power, cooling, connectivity, modularity and installation considerations within a coordinated infrastructure solution to simplify deployment and remain open to the changing operational demands of the data centre.