Based on your location, we think there is a website better suited to you.

Tate Global AMER

Sealing the Deal: Containment as the Key to Cooling AI

AI workloads are reshaping data center thermal design

Rack densities that once sat comfortably below 15 kilowatts are now pushing past 100 kW+ in high-performance environments. As heat loads climb, cooling strategies are shifting from selecting individual technologies to building system infrastructure that can evolve as density continues to rise.

At Tate, this systems-first approach is central to The Home of Data: creating environments where airflow, cooling, power, and containment operate as a unified platform rather than isolated components.

Much of the industry conversation has focused on the rise of liquid cooling. Yet the Uptime Institute Cooling Systems Survey 2025 shows that most facilities still rely primarily on traditional air cooling. While high rack density is accelerating interest in liquid technologies, integration complexity, cost, supply chain concerns, time to market, and operational risk remain significant concerns.

In practice, most operators are moving toward hybrid environments, supplementing air cooling with liquid where density demands it. This shift makes precise airflow control increasingly critical. Predictable separation of hot and cold air allows air-based systems to remain effective even as advanced cooling is introduced.

Containment provides that control, and becomes the constant that stabilizes thermal performance as cooling technologies evolve around it.

Making Hybrid Cooling Work in Practice

Most operators are not abandoning air cooling. Instead, they are selectively supplementing it with liquid technologies where rack density demands it.

This introduces a clear integration challenge.

Advanced cooling systems perform best when airflow behaves predictably. Without containment, hot exhaust can migrate across rows, cold air can bypass equipment, and localized liquid cooling can disrupt room-level balance.

With containment in place, hybrid deployments become more controlled. Operators can:

  • Apply liquid cooling only where required
  • Maintain efficient air cooling across the rest of the hall
  • Prevent thermal interference between systems
  • Expand high-density zones incrementally

In this model, containment becomes the permanent structural framework of the aisle. As density increases, operators can introduce liquid-cooled racks incrementally, often requiring only manifold valve activation and hose connectors, without altering the containment architecture.

At lower rack densities, containment was often treated as an efficiency measure. In high-density hybrid environments, it functions as operating infrastructure that allows data centers to pivot to liquid cooled deployments without data hall redesign  — by stabilizing inlet temperatures, protecting airflow integrity, and reducing the risk that incremental cooling changes ripple across the hall.

Research from the Uptime Institute consistently shows that ease of integration influences liquid cooling adoption. By stabilizing airflow, containment reduces the complexity and risk of hybrid deployments.  When paired with intelligent infrastructure platforms that provide real-time visibility into airflow and thermal conditions, such as Konnect by Tate, operators gain the data needed to validate performance as density increases.

Designing for Density and Change

Containment is typically implemented through hot aisle or cold aisle configurations.

Hot aisle containment captures exhaust air at the source and returns it to overhead plenums, making it well suited for high-density and hybrid layouts. Cold aisle containment protects supply air before it reaches IT equipment and remains common in raised-floor environments.

Regardless of configuration, adaptability is the priority. As rack densities climb, containment must support mixed workloads, phased liquid adoption, modular expansion, and retrofits with minimal disruption.

Long-term infrastructure value increasingly depends on accommodating change without repeated redesign. Designing with a hybrid approach in mind at the onset of data center projects helps to eliminate downtime and increase speed to market for data center operators.

 A Lower-Risk Path to AI Readiness

Few facilities will be rebuilt from the ground up for AI workloads. Most will modernize incrementally — adding density, introducing liquid cooling, and expanding capacity in phases.

Industry groups such as iMasons and analysts at Gartner consistently point to modular, adaptable infrastructure as central to scaling AI environments. In this context, containment functions as the thermal backbone of the modular data center, establishing controlled airflow zones that can support phased densification without repeated redesign.

By stabilizing airflow conditions early, operators can extend the useful life of air-cooled systems, introduce liquid cooling where required, and reduce the risk associated with ongoing retrofits.

Precision Enables Progress

AI is increasing both heat output and system complexity. Higher rack densities and mixed cooling architectures demand far tighter airflow control than legacy designs were built to provide. 

Containment delivers that stability.

By creating defined thermal zones and allowing air and liquid cooling systems to operate side by side, containment has become a core element of high-density data center design. It may draw less attention than emerging liquid technologies, but it increasingly determines how effectively those systems perform in real-world environments.

As infrastructure requirements continue to evolve, precise airflow management will remain central to reliability and scalability. When paired with intelligent infrastructure platforms that provide real-time visibility into thermal conditions — such as Konnect by Tate — containment not only stabilizes performance, but gives operators the operational insight needed to scale with confidence.