Based on your location, we think there is a website better suited to you.

Tate Global AMER
Knowledge Articles

What is Cradle to Cradle Certified® and Why Does it Matter?

Cradle to Cradle Certified® is a globally recognised, science-based certification programme for designing and manufacturing products that are safe, circular, and responsibly made. 

Unlike traditional sustainability models that focus on reducing harm, Cradle to Cradle Certified® supports circular economy product design — encouraging manufacturers to create products with positive environmental and social impact from the outset. 

Products are assessed across five performance categories: 

  • Material Health – Safe materials for people and the environment 
  • Material Reutilisation – Designing for reuse, recovery, and circular material flows 
  • Renewable Energy & Carbon Management – Reducing carbon and increasing renewable energy use 
  • Water Stewardship – Responsible water management 
  • Social Fairness – Ethical labour and responsible supply chains 

Certification levels range from Bronze to Platinum, reflecting increasing levels of verified sustainability performance. 

What Does Cradle to Cradle Certified® Silver Mean? 

A Cradle to Cradle Certified® Silver (v3.1) rating demonstrates verified performance across multiple sustainability criteria. 

At Silver level, manufacturers must show: 

  • Active circular material strategies 
  • Responsible social and ethical supply chain practices 
  • Implemented sustainability measures — not aspirational targets 

Silver certification is widely recognised within the construction sector as a meaningful step toward circular economy manufacturing and responsible production. 

Cradle to Cradle Certification for Raised Access Flooring

Tate’s RMG600 and RMG600+ raised access panels have achieved Cradle to Cradle Certified® Silver under certification number 7236. 

The RMG600 has a third-party verified EPD, HPD, VOC-tested, as well as Cradle to Cradle® Certified Silver. These credentials support key environmental frameworks including LEED v4, BREEAM, and WELL v2, making them ideal for commercial developments focusing on the highest environmental and user wellbeing standards. 

The RMG600+ is an award-winning panel manufactured with more than 91% recycled content, including low-carbon electric arc furnace steel. The floor panels were also recently awarded the One Click LCA Excellence Award in Low Carbon Manufacturing Certificate. 

The Cradle to Cradle assessment was independently conducted by Eco Intelligent Growth and verified under the Cradle to Cradle Certified® Products Programme (v3.1). 

The certification recognises performance particularly in: 

  • Material Reutilisation 
  • Social Fairness 

These categories reflect our commitment to lifecycle responsibility and ethical manufacturing within the built environment. 

Circular Manufacturing

How Tate Supports Material Reuse and Waste Reduction

A key contributor to our certification performance is our Take Back Scheme, supporting circular material recovery in raised access floor manufacturing. 

Through this approach: 

  • Steel from wood core access floor panels is separated and recycled into new steel products or reused. 
  • Wood core material unsuitable for reuse is shredded onsite and repurposed as biomass fuel. 
  • Three onsite biomass boilers generate approximately 3,000 megawatts of renewable energy per year to support manufacturing. 

This closed-loop approach integrates: 

  • Waste reduction 
  • Material recovery 
  • Renewable energy generation 
  • Lower operational carbon impact 

It demonstrates how circular economy principles can be embedded directly into construction product manufacturing. 

Planet Passionate

Sustainable Raised Access Flooring

Tate’s Cradle to Cradle Certified® Silver accreditation aligns with the broader sustainability commitments within our global Planet Passionate programme. 

This strategy focuses on: 

  • Energy efficiency 
  • Carbon reduction 
  • Water stewardship 
  • Circularity 

These priorities support the development of sustainable construction products designed to deliver long-term environmental and social value. 

Cradle to Cradle Certification as part of Continuous Sustainability Improvement

Cradle to Cradle Certified® is structured to promote continuous improvement. Each certification level acts as a benchmark for ongoing progress rather than a final endpoint. 

Achieving Silver reflects verified performance today while supporting further advancement toward higher levels of circularity and environmental responsibility. For us, this certification represents one step within a wider sustainability journey focused on measurable, science-based progress. 

FOOTNOTE 

Tate has achieved Cradle to Cradle Certified® Silver for these Raised Access Flooring Panels under certification number 7236. Cradle to Cradle Certified® is a registered trademark of the Cradle to Cradle Products Innovation Institute. Cradle to Cradle Certified® is the world’s most advanced science-based, multi-attribute certification programme for designing, making, and verifying materials and products that are safe, circular, and responsibly made. 

Note: the Cradle to Cradle Certified® Silver award was first announced prior to Kingspan Data Solutions’ rebrand as Tate.