Rapid growth in digital infrastructure is intensifying pressure on data centres to deliver maximum output while curbing environmental impact.
Sustainability now routinely drives design and operational direction but there are still hidden gains to be made, with some of the biggest carbon reduction opportunities lying in often-overlooked construction decisions made long before a facility becomes operational. These early decisions and their results can significantly shape a data centre's overall carbon footprint.
A recent Tate Europe project for a London-based colocation customer achieved a remarkable carbon saving of 347 tonnes of CO₂ and 59% reduction in embodied carbon by shifting focus to the ceilings, reimagining ceiling design and manufacture through a sustainability lens.
Driving Sustainability Through Innovative Design
By recommending a high-performance aluminium ceiling solution as a more sustainable alternative to traditional structural ceiling designs, we introduced flexibility and reduced material requirements during manufacture and installation phases.
To make a broader impact, we extended our sustainability focus from design to production; to achieve our 59% reduction in embodied carbon, Tate's Dublin manufacturing facility sourced raw materials from suppliers that utilise hydropower during production.
In maximising the impact of low-carbon design choices, integrated thinking is key. Tate's converged, turnkey infrastructure solutions guarantee our long-term project involvement and with it the opportunity to identify carbon reduction opportunities at every stage of the lifecycle. We're across early design and material selection through to construction, commissioning and ongoing operation, and this presence pays dividends in the form of unlocking less obvious opportunities for carbon savings.
Reducing embodied carbon – the emissions associated with the manufacture, transportation and installation of building materials – is one of the biggest challenges facing today's construction industry. As sustainability targets tighten and many of the more accessible carbon reduction measures have already been implemented, further progress is becoming harder to achieve. Operational efficiency often receives significant attention, but embodied carbon represents a major portion of a building's total environmental footprint, and therefore reducing it is an increasingly important focus area for the industry.
Optimising both the design and manufacture of this solution led to a
reduction in embodied carbon
Measuring Our Impact
Robust measurement and verification to prove real-world impact underpin meaningful sustainability measurement. In recent years, the construction sector has placed greater emphasis on transparent environmental reporting, enabling businesses to make informed decisions based on reliable data.
The results achieved in this project provide a clear example of measurable sustainability gains. Traditional ceiling systems can embody approximately 49 kg of CO₂ per square metre, while Tate's structural ceiling system achieved just 20 kg CO₂ per square metre. Independently verified through an Environmental Product Declaration (EPD), these figures provide confidence that the reported environmental benefits are based on recognised industry standards.
The Power of Collaboration
Stakeholder communication and collaboration were key drivers of this project. Sustainable outcomes are rarely achieved by a single organisation working independently. Instead, they require multiple stakeholders to share objectives, exchange expertise and remain committed to environmental goals throughout the project lifecycle.
Early engagement and open communication between Tate Europe, the general contractor and the customer's internal teams allowed the project team to identify opportunities for carbon reduction before construction began, ensuring sustainability considerations were integrated into every stage of decision-making.
Going forward, collaboration enabled the project team to make informed decisions that delivered both environmental and commercial benefits. Rather than treating sustainability as a compliance exercise, the partners viewed it as an opportunity to innovate and create long-term value.
The takeaway for the data centre sector is that achieving meaningful environmental progress requires more than adopting individual sustainable products, no matter how innovative. It demands a culture of cooperation where clients, contractors, manufacturers and suppliers work together to challenge conventional practices and explore better alternatives – alternatives that aren't necessarily radical transformations, but smaller opportunities for optimisation that can deliver significant carbon reductions while maintaining the performance, reliability and flexibility required. From ceiling to floor, every component matters.
The success of this project sets a powerful benchmark for sustainable construction within the industry. By combining innovative low-carbon solutions with strong stakeholder collaboration, the team demonstrated that significant reductions in embodied carbon are both achievable and practical. The project also reflects Tate's commitment to Planet Passionate, the company's global sustainability programme focused on reducing carbon emissions, advancing circularity, and driving positive environmental change across the built environment. As sustainability continues to shape the future of construction, solutions like those delivered by this project provide a blueprint for how organisations can reduce environmental impact while delivering high-performing infrastructure that supports a more sustainable future.