Material Selection: Your Manifold Material Choice Determines System Reliability

Material Selection

Why Material Selection Matters

Every liquid-cooled rack in an AI-ready data centre depends on a manifold to move coolant where it needs to go, and the material behind that manifold is one of the biggest reliability factors a project decision makes. Liquid cooling is now baseline infrastructure in hyperscale data centres, driven by AI, GPU and HPC deployments that exceed the limits of air cooling. Liquid cooling loops have become long-life infrastructure assets, with reliability expectations that match mechanical plant systems.

Manifolds sit at the interface between facility plant, CDUs and rack-level cooling hardware, meaning the material directly affects hydraulic performance, leakage risk, QA and long-term system stability. The same holds for every layout Tate builds, from ceiling-supported and in-aisle configurations to underfloor and floor-supported ones.

Manifold Options in an APAC Deployment

Tate's Australian and Asia-Pacific manifold range covers four options, and the same material principles apply to all of them. Ceiling Supported Manifolds suit air- and liquid-cooled racks under Tate Forte LEC structural ceilings, In Aisle Manifolds integrate within Hot Aisle Containment for high-density rows, Underfloor Manifolds suit new-build and retrofit projects routed beneath raised access floors, and Floor Supported and Custom Configurations handle site-specific constraints. Whatever the layout, the manifold material is what determines how the system performs over its working life.

Steel: The Clear Choice for Data Centre Manifolds

Meeting Australian Standards

In Australia, welded stainless steel construction of this kind is assessed against AS 4041 (Pressure Piping) for pressure pipework design and construction, with AS/NZS ISO 3834 and AS/NZS 1554.6 governing welding quality management and stainless steel welding practice. These are the local standards Australian mechanical and process engineers reference alongside the ASME codes used across Tate's manufacturing.

The Tate Difference

Proven Delivery at Scale

Over 1 GW of liquid cooling piping delivered for hyperscale, high‑density deployments.

Modular, Pre‑Fabricated Steel Systems

Manifolds are manufactured from 304 stainless steel in pipe diameters from 50mm to 200mm, fully pre-fabricated, pressure-tested, and cleanliness-verified before they leave the factory, with ball or butterfly isolation valves and full documentation and traceability from production through to installation.

Optimised for Fast Track Builds

Flanged modular assemblies install quickly with no field welding, reducing programme risk and site hours.

Engineered for High Density Cooling

Steel delivers predictable, stable performance with cleaner routing, fewer joints, and long‑term reliability under thermal and pressure cycling.

For assured performance and long term stability, stainless steel remains the most trusted material for mission critical data centre cooling.

Discover the Full Insights

Want to learn more? Read the whitepaper or connect with our team directly.